Revit content zip files from Daikin Applied are freely available and 
do not require a password to unzip.

In order to make Revit files that are both compliant with the 
Autodesk Revit Model Content Style Guide and also that are intuitive and 
easy to use, the file names and subfolders must have descriptive (long) names.

This may cause any of the following issues during the unzipping process:


1)  On all versions of Windows you should unzip these files to a higher-level 
folder (with a short name) such as:   

C:\Temp

Unzipping to a lower-level folder, such as to your Desktop, may cause errors 
because the final extracted file locations may be too long for Windows to handle.  

On Windows XP this error may falsely appear in the form of asking you for a 
password to unzip the files.


2) If you are using Windows XP's built-in uncompression tools, an issue exists 
in Windows XP itself when long file names are embedded in a zip file.  This issue 
can falsely cause Windows XP to ask you for a password to unzip the files.  

This issue does not exist on Windows Vista or later.

To correctly unzip any problematic files on Windows XP, either:

 - Use a third-party uncompression tool, or

 - Right-click on the zip file and select the "Extract All..." pop-up menu 
choice.  This will start a wizard which will correctly unzip the content files.